Controllers by ESPEC:

Primary process controllers on ESPEC chambers


P-300

Flagship controller used on most ESPEC North America chambers (except benchtops).

  • Touch-screen
  • USB access

See more on the P-300


GL

Flagship controller used on ESPEC North America Platinous & Global-N Chambers. Also as an add-on to chambers going back 30 years.

  • Touch-screen
  • Ethernet and Restful API
  • USB access

See more on the GL


P-200

Flagship controller used on the Benchtop Temperature & Humidity Chambers (SU/SH).

  • Touch-screen
  • USB & Ethernet access

See more on the P-200


Watlow F4T

Current controler for BT/Criterion benchtop chambers made in the USA.

  • Touch-screen 
  • Ethernet with Modbus

See more on the Watlow F4T

Recommended: Web Controller

The ESPEC Web Controller is an embedded server/software solution for monitoring and programming your chamber via Ethernet. Works with P-300, SCP-220, F4T, & F4 controllers. That’s most ESPEC North America chambers built since 1997.

Independent of the controller itself, the Web Controller adds additional capabilities for datalogging, programming, alarm emails, and RESTful API.

Try the live demo now!


Web Controller details


Self-install kit for existing units

Contact ESPEC North America

General requests sent from this page will be routed to the best party in our organization to help you. Please complete all fields to ensure a fast response.


Contacting ESPEC