ESPEC at the AFA Air, Space & Cyber Conference 2026
Tuesday, August 25 2026
We're exhibiting at the Air, Space & Cyber Conference this September in National Harbor, Maryland. With over 40 years of experience in aerospace environmental testing, this show puts us directly in front of the Air Force, Space Force, and defense industry teams who depend on that kind of depth.
Quick Facts
Dates: September 14-16, 2026 (Monday-Wednesday).
Venue: Gaylord National Resort and Convention Center, National Harbor, Maryland.
Theme: "Advancing Air and Space Dominance: An Urgent Call to Build and Sustain the Forces."
ESPEC Booth: 4412, Woodrow Wilson Ballroom.
Equipment on Display: TSE-12 Thermal Shock Chamber.
Registration: Free for U.S. uniformed military, Department of Defense civilian personnel, and military spouses.
Why We're Exhibiting
This year's theme is a force-structure and readiness message. Sustaining the forces means sustaining the hardware those forces operate, and that takes reliable, repeatable environmental qualification at every stage from component to system.
That's what our chambers and reliability systems are built to verify. We're the world's largest company dedicated exclusively to environmental test chambers, so every investment we make points at one thing: making reliability testable. For programs where failure carries mission consequences, that exclusive focus matters.
Environmental and Reliability Testing for Air Force, Space Force, and Defense Programs
Defense and aerospace qualification programs run against MIL-STD-810, RTCA DO-160, and AS9100. Your test equipment has to be up to those standards before your hardware can be.
Our portfolio covers the full range those frameworks demand, from benchtop electronics to walk-in and drive-in chambers for system-level qualification.
Thermal Shock and Altitude Testing for Aerospace Qualification
Rapid thermal transitions are one of the most common sources of failure in aerospace hardware. Our thermal shock chambers, including the TSE-12 and TSA series, subject components and assemblies to controlled temperature transitions that expose thermal fatigue in solder joints, connectors, and structural materials before they fail in the field.
When your program calls for avionics, missile, or spacecraft component qualification, these are the systems your team uses to prove the design holds.
Pressure matters as much as temperature for many aerospace applications. Our altitude chambers simulate reduced-pressure environments for avionics, guidance systems, and spacecraft assemblies, giving your team a repeatable way to verify performance at altitude before the hardware ever leaves the ground.
HALT and HASS: Finding Failures Before the Field Does
Avionics has been the largest segment for our HALT/HASS technology throughout our history in accelerated stress testing, and there's a clear reason. MIL-STD compliance testing confirms a design meets spec, but it doesn't tell you where your design margins are or what failure modes you've missed.
Highly Accelerated Life Testing applies combined stresses beyond spec limits to uncover those weaknesses early in development, when fixing them is still feasible. HASS then uses the limits HALT establishes to screen production units against supply chain drift, counterfeit components, and process variation.
To date, we remain the only OEM to offer HALT/HASS services to our own customers. If your program needs to build or recover that capability, our Solutions Group can design and implement it. Explore our HALT/HASS product family or the full Qualmark HALT/HASS systems to see what we bring to accelerated reliability programs.
AMI/AMR and HAST: Semiconductor and PCB Reliability for Defense Electronics
Defense electronics increasingly depend on high-density PCBs, advanced semiconductors, and miniaturized avionics assemblies where electrochemical migration and solder joint failures carry direct mission risk. Our AMI/AMR electronic reliability systems give you continuous, high-precision monitoring of electrochemical migration and conductor resistance under real test conditions, not spot checks after the fact.
Paired with our HAST chambers, which compress weeks of humidity qualification into hours by combining elevated temperature, humidity, and pressure, your team can qualify defense electronics assemblies faster without giving up data integrity.
CMMC Level 2 Certified: What That Means for Defense Industrial Base Customers
We achieved CMMC Level 2 certification with a perfect score of 110 out of 110, with no findings requiring a Plan of Action and Milestones. Under CMMC 2.0, which entered Phase 1 implementation on November 10, 2025, prime contractors have to verify that subcontractors hold current certification before sharing Controlled Unclassified Information.
When your procurement team needs a testing partner you can share program details with, we meet that requirement. It's a verifiable procurement qualification, not a marketing claim.
Supporting Defense Test Labs Beyond the Equipment Sale
Your lab's audit readiness and uptime don't depend only on the chamber you buy. They depend on what happens after installation.
Our Chamber Care preventative maintenance program, ISO/IEC 17025:2017 accredited calibration services, and responsive field service are built to keep defense test labs performing under the schedule pressure and audit scrutiny that define this sector. Our operations in Hudsonville, Michigan and Aurora, Colorado both hold ISO 9001:2015 certification.
As our brand messaging puts it: "Our relationship with the customer begins once the product is delivered. We stand by our clients with training, calibration, and responsive service throughout the entire lifecycle of their chamber." To learn more about our certifications and service model, visit the ESPEC North America about page.
Schedule a Meeting at the 2026 Air, Space & Cyber Conference
We'll be at booth 4412 in the Woodrow Wilson Ballroom, with the TSE-12 Thermal Shock Chamber on the floor. Stop by to see the system in person, talk through your program qualification requirements, walk through chamber selection for your application, or discuss building or strengthening a HALT/HASS program. Our technical team is there to have real conversations, not deliver a product pitch.
If you'd rather connect before the show, reach out now to schedule a pre-event consultation. It's an easier way to make sure the time you spend at our booth is focused on what your program actually needs.
About the AFA Air, Space & Cyber Conference
The Air & Space Forces Association's annual Air, Space & Cyber Conference is the premier professional development event for the U.S. Air Force and Space Force, and it draws defense contractors, government officials, and industry technology leaders alongside them. The 2026 conference runs September 14-16 at the Gaylord National Resort and Convention Center in National Harbor, Maryland.
Both in-person and virtual attendance are available, with main ballroom sessions streaming for virtual attendees. Free registration for U.S. uniformed military, DoD civilian personnel, and military spouses makes it one of the most accessible forums on the defense industry calendar.