The Role of HALT and HASS in Enhancing Vehicle Safety and Performance

Monday, October 28 2024

Vehicle safety and reliability are paramount in the automotive industry. Every time a vehicle is driven or involved in an accident, its true durability is tested. To ensure that your automobiles are fully prepared for these real-world challenges, implementing HALT (Highly Accelerated Life Testing) and HASS (Highly Accelerated Stress Screening) on critical sub-assemblies is essential.

These rigorous testing methods provide invaluable insights, allowing you to make informed decisions about how to enhance your vehicle’s safety and performance before it hits the market. By incorporating failure-oriented stress-testing using HALT and HASS, you can ensure that the critical components in your vehicles are ruggedized to their fullest extent.

What Is HALT?

HALT, or Highly Accelerated Life Testing, was developed in 1969 by Dr. Gregg Hobbs and has since become the standard for maximizing subassembly durability and reliability. This rigorous testing methodology evaluates how well vehicle components can withstand extreme conditions, subjecting the subassemblies to stresses far beyond what they will see in the field to rapidly expose potential weaknesses.

The primary purpose of HALT in the automotive industry is to expose failure points early in the design process, ultimately maximizing subassembly reliability. By identifying these vulnerabilities before the vehicle reaches the market, manufacturers can ensure that their automobiles are well-prepared for the challenges of everyday driving.

HALT Testing Methodology

  • Temperature Stress Testing: Determines the highest and lowest temperatures a vehicle component can endure before becoming damaged or unusable.

  • Rapid Temperature Cycling: Rapidly shifts between the extreme temperatures identified in the previous step to establish the component's ability to withstand sudden changes in temperature.

  • Vibration Step Testing: Subjects components and subassemblies to intense vibration until the operational and destruct limits of the device are defined.

  • Combined Testing: Integrates the above stresses into a single, comprehensive test to subject the component or subassemblies to maximum level stresses to uncover all possible failure mechanisms.

    Benefits of HALT Testing

    HALT testing is designed to push a product to its limits, identifying weaknesses by testing it until it fails. This approach provides several key benefits:

    • Identifying Product Weaknesses: By uncovering design flaws in subassemblies, engineers and quality assurance teams can make necessary improvements, enhancing the overall safety and performance of the vehicle.

    • Reducing Field Failures: Preventing failures before they occur reduces customer complaints, warranty complaints, and potential recalls.

    • Improving Product Quality: A more reliable product fosters a strong brand reputation, leading customers to trust your brand and expect exceptional quality with future releases.

    What Is HASS?

    HASS, or Highly Accelerated Stress Screening, is a testing methodology used to identify defects that may creep into the subassembly during manufacturing. Unlike HALT, which subjects components to extreme conditions and stresses the unit under test to failure, HASS is designed to screen products before they are shipped using stresses similar to those used in HALT but at lower levels so that any new weaknesses can be exposed.

    HASS Testing Methodologies

    • HALT must be completed before HASS begins to identify the operating and destruct limits for the unit under test and identifying the safe levels that can be used in production. These stresses are used to screen 100% of the units before shipment.

    • Combined Testing: Subjects the unit to thermal and repetitive shock vibration stresses simultaneously, maximizing the total stress and fatigue to the unit.

    • The goal is to make the screen as time-efficient and as effective as possible; a combined stress environment will meet these needs.

    Benefits of HASS Testing

    • Manufacturing Defect Detection: By identifying defects before a unit is built into a vehicle, HASS reduces the likelihood of customer service issues and warranty claims, leading to lower overall costs.

    • Improved Product Quality: Detecting and addressing defects before the product reaches the market enhances its quality, contributing to a reputation for reliability and positively impacting your brand’s image.

    • Cost Savings: Finding defects before they escape into the field will dramatically reduce the cost impact of the defect(s).

    Ready to Improve Product Reliability Fast with ESPEC?

    At ESPEC, our state-of-the-art testing facilities and chambers are designed to uncover potential failure points in your product. Identifying these areas for improvement is essential to creating a top-quality vehicle. Let us be your partner in ensuring vehicle component safety and reliability. Learn more about how our HALT testing facilities can provide peace of mind as your vehicles enter the market by reaching out today.