P-300 programmer/controller simulation
Just click on the 'screen' as if you were operating an ESPEC chamber to explore all this controller can do.
Constant Mode Set-up (Main)
When a single temperature/humidity setting needs to be run constantly,
choose the Constant mode. From this screen you can save three different
constant setups, each which can be named for easy reference.
You can click on the SP (set point) values to change them, or choose
'Details' to change associated settings.
NEW: Three constant setups can be saved instead of one.