Web Controller Live Demo

You are about to enter a live demonstration of the ESPEC Web Controller an embedded server/software solution that allows monitoring, programming, "Internet of Things" functionality, and easier datalogging on your chamber via PC on your network. You are welcome to make changes as if you were using a real chamber.

Login as "Administrator" to see most functions:

User: "demo" 
Password: "demo"

Full documentation including manual & API at bitbucket.org

About the demo:
This demonstration uses an actual Web Controller connected to a running SCP-220 programmer/controller at ESPEC's facility. Because the controller is not connected to a chamber, the temperature or humidity does not change in response to the setpoint, and you will not see any alarm notifications. The Web Controller also works with ESPEC P-300 and Watlow F4T & F4 programmer/controllers.